Home » Raritan Blog
Minder Singh
August 14, 2014
Power distribution Units or PDUs really boil down to two types: basic and intelligent PDUs (or more succinctly, iPDUs). Basic PDUs merely deliver power to IT devices. Aside from that, basic PDUs don’t bring much else to the table. iPDUs on the other hand, provide a number of innovative features that can help data centers manage their energy resources more effectively. Here are some of the most important features that set iPDUs apart from basic PDUs.
Richard Dominach
July 29, 2014
A common question I get is: what is the difference between the new Dominion KX III and the previous generation KX II KVM-over-IP systems? The short answer is: KX III is our next generation KVM-over-IP switch family that is compatible with the KX II, can do virtually everything the KX II can do (at the same price point), but with dramatically improved performance and support. The KX III is compatible with the KX II in terms of user features, the user interface, CIMS (server dongles) and CommandCenter management. Here are some other notable features.
Michael Bord
July 23, 2014
Every Raritan intelligent rack PDU comes equipped with USB ports that allow users to perform a variety of amazing tasks. But, for some reason, USB ports don’t fill most people with much excitement. The USB port has become the technology analog to vanilla, or at the very least to claiming that a ‘thing’ is vanilla: bland, commonplace, and ordinary. It was developed back in 1994 by a computing giant's roster that included: Compaq, Dell, IBM, Intel, and Microsoft; all of whom had the goal of providing an easier way to connect external devices to personal computers.
Hugo Lin
July 21, 2014
A KVM Switch is a hardware device that allows you to control multiple computers via a single keyboard, monitor, and mouse (KVM). The first KVM switch was created as a testing tool for motherboard and production server quality tests, and only supported video and keyboard since the mouse hadn’t been invented at that time. And as computer technology continued to evolve, so did KVM switches which led to the development of a variety of types for different systems and applications. Here are the four categories of KVM switches.
Paula Alves
July 16, 2014
Raritan’s dcTrack® DCIM Operations Software has been nominated for the 2014 People’s Choice Stevie® Awards for Favorite New Product! Now, if you’re unfamiliar with Raritan and dcTrack, you may be wondering what makes this DCIM solution, among so many solutions on the market, such a powerful resource for data center operators. Three reasons data center operators have had so much success with the tool are that it provides them with better capacity management and accurate asset management, and automates manual processes.