Home » Raritan Blog
Michael Bord
March 10, 2016
This month we are thrilled to introduce Raritan’s new logo. Raritan Inc. is now Raritan, a Brand of Legrand. On the surface, it would appear to be nothing more than semantics and a sleek new modern design. But, there’s more to the story than that.
David Wood
February 16, 2016
This past week, we opened our mailbag and found the following customer email:
Dear Raritan team,
We mostly love the 16A rated rack transfer switch so far! The physical design made it easy to connect power feeds from the back of the cabinet. The outlet-level metering and switching let us power off development servers no one was using on weeknights and weekends. But, here’s one thing that wasn’t so great:
We recently experienced a total device failure. We weren’t sure what it was at first, but quickly realized it was a blown fuse from both the web interface and indicator lamp/alarm on the unit. Once we replaced the fuse the unit continued operating just fine. But, why is it there in the first place? And why not have a circuit breaker instead of a fuse?
Tl;dr What is the purpose of the fuses located on the inlet side of Raritan’s rack transfer switch and why not have a circuit breaker instead?
Michael Bord
January 4, 2016
Originally Published in Processor.com on April 27, 2015
IT managers have a lot on their plates when it comes to managing servers both in-house and remotely, especially if they work in environments where they need access to multiple systems regardless of whether they are onsite or at a separate location. Fortunately, there are plenty of solutions to consider for remote server management that is unique from one another but can also be used together in certain situations to cover all of your bases.
Michael Bord
August 25, 2015
Paula Alves
July 9, 2015
Catch the free replay of the webinar moderated by IDC on July 16, 2015 2PM EST
IDC’s Jennifer Koppy leads an interactive webinar with data center leaders at UF Health Shands Hospital and CareTech Solutions. Learn how to get buy-in from stakeholders, breakdown silos, increase collaboration, and slash 50% on data center OPEX. Discover how to drive change from day one, and set yourself up for more success well into the future.
To watch the replay click on the link below.