Home » Raritan Blog
Jessica Ciesla
February 7, 2019
It's no secret that machine learning has infiltrated everything from the technology sector to the consumer market. From smartphone assistants to Google's Artificial Intelligence (AI) advancements, machine learning continues to help tackle the most challenging problems in the world. When it comes to data centers, the use of machine learning has led to incredible advances in efficient and reduced energy consumption.
Google's AI Leads To A Breakthrough In Energy Consumption
Google's DeepMind AI program has been used in their data centers to reduce the amount of energy used on a daily basis. The implications of this type of machine learning are potentially industry-changing. Take for example the amount of energy that is used to cool a data center. From cooling the servers to maintaining the optimal temperatures in a rapidly warming world, data centers require an astronomical level of energy to cool. Fortunately, AI programs, like DeepMind, are designed to not only reduce the amount of energy needed to cool a data center, but to also provide actionable insights into a global issue: climate changes.
Jessica Ciesla
January 30, 2019
Content originally sources from IDC.
As discussed in Part 1 of this series, traditional data centers must prepare for future changes and challenges within the industry. These changes include the impacts of emerging technologies, higher costs, and environmental concerns. As a direct response to these changes, data centers will need to respond to three influential factors as they seek to increase operational efficiencies in the years to come.
Influential Factor Recap
In the first part of this series, we discussed the three key factors that will influence the future of data centers in the coming years. These three factors include:
Jessica Ciesla
January 23, 2019
Data center managers need to leverage the right tools if they want to successfully monitor mission critical IT devices. However, in an effort to reduce costs, far too often data center managers are tempted into taking unnecessary risks that not only threaten business continuity but put the entire infrastructure at risk. Fortunately, through best practice approaches, these risks can be mitigated and the optimal levels of environmental monitoring can be achieved.
Jessica Ciesla
January 17, 2019
Content originally sourced from IDC.
Traditional data centers must prepare for future changes to the industry. In fact, it's no longer a matter of "if" but "when" these changes will occur. As the amount of data that is consumed each day increases, so too will data centers need to increase their operational efficiencies as they respond to challenges associated with emerging technologies, environmental concerns, and higher costs.
Jessica Ciesla
January 8, 2019
Did you know that data centers represent an impressive 1.8 percent of the total energy consumption within the United States? As anyone knows, energy consumption is expensive. The challenge for many data centers is that future energy usage is expected to continue to increase (as will their respective costs). This challenge is further escalated by the fact that many data centers are ineffectively using what energy resources they do have.