Home » Raritan Blog
Jessica Ciesla
May 16, 2019
It's no secret that data centers have copious amounts of IT equipment. However, the challenge that data center managers face on a daily basis is knowing how to properly monitor and react (in real time) to each piece of IT equipment. The good news is that intelligent PDUs can help data center managers successfully monitor inlet, outlet, and circuit breaker metering. As any seasoned data center manager will tell you, inlet, outlet, and circuit breaker metering is critical to avoiding downtime, effectively utilizing power resources, and reducing data center costs year over year.
Jessica Ciesla
May 6, 2019
Did you know that data centers consume approximately 1.8 percent of the total United States' electricity consumption? This unprecedented energy usage is expected to increase year over year as the amount of data consumed on an annual basis rises at unparalleled rates. The inherent challenge of rising energy and data consumption levels lies in environmental monitoring. In fact, when IT equipment isn't operated in the right environment (including within the designated temperature safe zone) it can lead to disastrous results.
Jessica Ciesla
April 18, 2019
With each passing year data center power infrastructures become more complex. In fact, data is expected to reach an unprecedented 163 zettabytes by 2025, which means that data center operators must figure out how to a) support the additional data, b) reduce costs, c) increase efficiencies, and d) remain energy efficient. Fortunately, data center operators can address the latter challenges with the help of the advanced power metering and data management technologies found in Intelligent PDUs.
Jessica Ciesla
April 4, 2019
The Dominion KX IV-101 represents the latest in a long series of innovations from the Raritan team. In fact, the Dominion KX IV-101 is our fourth generation Dominion KVM-over-IP switch. It delivers an unparalleled level of power, supports Java-free access from anywhere, and offers BIOS-level remote access to PCs, workstations, and servers. With 4K video resolution at up to 30 frames per second in 4🔢2 color, the Dominion KX IV-101 redefines the remote management that many businesses need to thrive.
Enjoy The Most Popular Dominion Features
The beauty of the recently released Dominion KX IV-101 is that it allows businesses to enjoy un-blocked, high performance access to equipment via the Dominion User Station, PCs, or laptops. This impressive KVM-over-IP switch also allows users to enjoy the most popular Dominion features, including:
Jessica Ciesla
March 25, 2019
Data centers throughout the globe are constantly finding new ways to innovate. More often than not, these innovative approaches stem from a growing need to reduce unexpected downtime, increase efficiencies, streamline operations, and optimize the entire data center for future growth. While you most often hear about enhancements to DCIM solutions or the benefits of intelligent rack PDUs, one topic that isn't covered as often are outlet types including C21 / C22.