Home » Raritan Blog
Jessica Ciesla
July 15, 2020
Raritan's PX3 PDUs monitor a variety of electrical and environmental parameters. You can receive alerts on anything that gets monitored – inlet data, outlet data, circuit breaker status, unbalanced loads, and power factor, to name a few. To configure and receive alerts successfully, you need to ensure the following actions have been completed:
1. Configure Alert Delivery Mechanism – how to set up and receive your alerts: SNMP and/or SMTP.
a. If you prefer your alerts to be sent to an SNMP manager tool, you need to enable: Device Settings > SNMP > Enable SNMP Notifications
It is important to note that this setting is different from the SNMP Agent setting. You won't be receiving SNMP alerts even if you have enabled SNMP v1/ v2c if you don't explicitly enable SNMP Notifications.
Jessica Ciesla
June 15, 2020
The COVID-19 pandemic is an evolving world-wide public-health and economic crisis. Companies must keep their business operations and systems running. They also need to keep their employees safe and healthy. Many employees are now working from home, either on a full or part-time basis. While the worst seems to be behind us in much of the United States, Europe, and Asia, the Center for Disease Control (CDC) is warning that there may be a “second wave” in the fall/winter. Remote management can be of enormous benefit in this type of uncertain environment.
Jessica Ciesla
April 2, 2020
Looking for an economical KVM solution? This blog discusses features included in the new Dominion LX II, and why it would be beneficial for you to trade up from the original Dominion LX.
The new Dominion LX II from Raritan is the latest in a line of products designed with the small to midsize business IP KVM switch user in mind. Our new unit is designed to provide economical, Java-free, BIOS-level remote access to between 8 and 16 servers as well as virtual media. The new Dominion also supports connections up to 15 frames-per-second at a resolution up to 1080p and 1200p. With six different options available, the next generation LX II is poised to become the leading SMB IP KVM switch on the market today.
Jessica Ciesla
March 18, 2020
In these uncertain times, when business operations are threatened, remote management tools can help to keep vital IT infrastructure running and to respond to emergencies. Remote management, by enabling employees to work from home, can be of enormous benefit. Raritan recommends that our customers immediately review the state of their remote management tools to prepare for their use in this emergency. We have created this checklist to use in your planning.
Jessica Ciesla
February 5, 2020
Looking for an economical KVM solution? This blog from Raritan discusses the Dominion LX II, an IP KVM switch designed for small to midsized businesses (SMB).
The new Dominion LX II from Raritan is the latest in a line of products designed with the small to midsize business IP KVM switch user in mind. Our new switches are designed to provide economical, Java-free, BIOS-level remote access to between 8 and 16 servers, as well as virtual media to copy files and install software. The new Dominion also supports connections up to 15 frames-per-second at resolutions up to 1080p and 1200p. With six different options available, the next generation LX II is poised to become the leading SMB IP KVM switch on the market today.