Home » Raritan Blog
September 3, 2010
Raritan Booth #118
September 12-15, 2010
MGM Grand Hotel & Convention Center
Las Vegas, Nevada
Greg More
August 30, 2010
Today’s high power demands, increasing power costs and constantly changing equipment require data center and facilities managers to look for power solutions that can deliver a lot of power but are flexible. A typical data center has both medium density (5-10 kW/rack) and high density (15-30 kW/rack) equipment racks. For example, some racks may have 2U/4U application and database servers, others may have 1U Web servers, still, others may support blade servers, storage networks, or high density networking fabric.
The power requirements for this variety of equipment can range from single phase to three phase, rack power (kW) may be anywhere from 5 kW to 30 kW per rack, and there could be dozens of different physical receptacles. The key is to efficiently utilize the available power capacity and to maintain uptime to the greatest extent possible while changes are made. The traditional approach uses pedestals at several locations in the data center with under-floor conduits or whips from the pedestal to racks. All the cable under that raised floor can impede airflow and cooling. The fixed feeds lead to decreased flexibility and challenging serviceability. In fact, it is not uncommon for some cables to be abandoned in place.
Allen Yang
August 26, 2010
Raritan IT team recently decided to change our naming and association schemes in Power IQ. This change reflects the new level of power usage details IT wants to track, and how we plan to utilize such information to measure energy savings from the investment in replacing old servers with new, more energy efficient IT equipment.
In the prior Power IQ naming scheme, we name the PX outlets by “phase-circuit-rack-L/R”. From this naming scheme, one can easily tell that it was PX-centric thinking. Using Power IQ, IT was able to easily know the total data center power consumption, as well as power usage by circuit and by the rack. The power consumption by individual IT devices was interesting but not as important for power capacity planning, especially when the servers were largely 1U/3U rack-mount servers.
Anthony Bonaventura
August 23, 2010
IT administrators in the government space are concerned about three things when they arrive at their place of work: security, security and security.
With the recent, and not so recent, cyber attacks on military and civilian agency networks, the government is constantly looking to the OEM and system integrator communities for new solutions to insure the lock-down of federal information system networks and servers that carry and hold information critical to the security of our nation.
Couple this daily challenge with compliance directives issued in large part by executive orders and shrinking budgets, data center managers hands are full. Not to mention that these folks have some of the busiest days out of anyone in the federal IT space.
Dorothy Ochs
August 11, 2010
Come visit the Raritan booth at DatacenterDynamics in Washington, DC on August 31st to learn about our intelligent energy management solutions. For more information and to register, visit https://www.datacenterdynamics.com/en/conferences/.