Home » Raritan Blog
Herman Chan
September 28, 2012
I read today that HP released its Proliant DL560 Gen8 Server Series with support for 4 Intel Xeon® CPUs, each CPU supporting 8, 6, or 4 cores. In addition, up to 1.5 TB of memory and 5 hot plug drives are supported. And, to boot, you get ALL this in a compact 2U package. That’s a lot of horsepower to help support increasing virtualized workloads.
Now, how would you power such a beast? Well, it comes with a pair of 1200W highly efficient 80 Plus rated power supplies. If you decide that you want to pack 20 of them in a 42U rack, you’d need to provision about 16KW of power to each rack in a rack iPDU with at least 20 C13 outlets. How did we get to 16KW? We made a simple assumption that the server may run @ 65% of nameplate or ~780 watts. 780 watts x 20 servers is just about 16KW. Your mileage will vary depending on what you decide to use as a nameplate de-rating assumption. Typical ranges fall somewhere between 60-70%. Given this, your choices to power a rack full of these will likely be one of 2 options depending on whether you’ve got 208V 3 phase or 400V 3 phase coming into the cabinets. They are: (A) a pair of 208V, 3 phase, 60A rack iPDUs providing 17.3KW of power or (B) a pair of 400V, 3 phase, 30A rack iPDUs providing 16.6KW of power. Check out our iPDU product selector to find the one that suits you.
Dorothy Ochs
September 27, 2012
Join us as we discuss how to successfully deploy high power to your racks, and how you can gain secure remote access to your data center
And stop by our booth (#644) to see our newest Power, DCIM and KVM solutions
Get a registration discount on us—Use code RARITANF12!
Register at http://www.datacenterworld.com/fall2012/
TWO PRESENTATIONS:
Effectively Deploying High Power in Data Centers
Date: Monday, October 1st at 2:30pm
Room: Lincoln C
Speaker: Greg More, Senior Product Marketing Manager at Raritan
Achieving Secure Remote and Local Access for Your Data Center
Date: Monday, October 1st at 9:45am
Room: Jackson CD
Speaker: Richard Dominach, Manager of KVM and Access Product Management at Raritan
We will have live demos at our booth (#644) and will be raffling an iPad. Be sure to stop by!
Event Details:
AFCOM Data Center World
Sep. 30th - Oct. 3rd
Gaylord Opryland Resort and Convention Center
Nashville, TN
Register now: http://www.datacenterworld.com/fall2012/
Paula Alves
September 19, 2012
Today Raritan released Dominion KX II-101-V2 Release 5.3, providing several enhancements that will delight both Government and non-Government users. With this new release, the Dominion KX II-101-V2 continues to be a leader in the one port KVM/IP class, offering the highest in video resolution, and becomes the only one in its class to offer mobile access (with CC-SG) and FIPS 140-2 encryption.
With mobile KVM access for iPhone and iPad, users can now access and control servers connected to the Dominion KX I-101-V2 via their Apple iPhones and iPads. This provides emergency 24x7 out-of-hours access, as well as convenient everyday access for iPad enthusiasts. CC-SG Release 5.2 or later is required for this capability.
To meet the changing technology needs of KVM customers, the Dominion KX II-101-V2 now supports High Definition (HD), 1080p remote video resolution. In addition, popular widescreen formats are supported including 1600x1200, 1680x1050 and 1440x900, so remote users can work with today’s higher resolution monitors.
For government, military and other high security applications, the Dominion KX II-101-V2 is the first device in its class to use a validated FIPS 140-2 Cryptographic Module for enhanced encryption. Modules tested and validated as conforming to FIPS 140-2 are accepted by federal agencies of the U.S. and Canada for the protection of sensitive information. Other security features, including IPv6, security banner, and SNMPv3 are also supported with this new release.
For more information, please access our website.
Dorothy Ochs
September 14, 2012
See how we can help:
- Reduce energy use and comply with Executive Order 13514
- Easily manage agency consolidation plans by tracking all of the assets in your data centers
- Provide you with secure remote access to server management
REGISTER NOW at
http://www.marinemilitaryexpos.com/modern-day-marine.shtml
EVENT DETAILS
What: Modern Day Marine
When: September 25-27, 2012
Where: MCB Quantico, VA
Dorothy Ochs
September 7, 2012
Raritan will be presenting at the DCIE (Data Center Innovation Expo) on September 18-19 in Montreal. You are invited to join us and stop by booth #101.
When: September 18th from 2:30 PM - 3:45 PM
Location: Room 514C
Title: DCIM, what is it and how is it helping data center managers today in improving operational and energy efficiencies?
Abstract: There has been a lot of buzz, hype, and confusion around DCIM (data center infrastructure management) software that has been created by both vendors and industry analysts in the past year. In this session you will learn how data center managers like yourself are actually filtering out this hype and confusion and are using DCIM to drive data center operational excellence. Once such scenario is to automate existing manual processes for managing moves, adds and changes (MACs). Another scenario enables managers to make better informed decisions using intelligence built into DCIM to reduce cooling energy costs. Both examples will be supported with real-world ROIs.
For more info and to register, visit http://www.datacenterinnovations.com/en/index.html.