Home » Raritan Blog
Richard Brooke
April 29, 2013
In my last post, I described the great volumes of power consumption and environmental data you can get from Raritan’s iPDUs, and how that can help you lower energy costs in the data center. We only scratched the surface, though, of the analytics and reporting capabilities of Power IQ software, and how it enables best practices in power management.
Some of the smarts we’ve put into Power IQ come right from the American Society of Heating, Refrigeration and Air-Conditioning Engineers (ASHRAE). Here, I’m referring to their Psychrometric chart, a guide to optimal temperature and humidity ranges for the data center. You can easily set these parameters to serve as notification thresholds for Raritan’s temperature and humidity probes, or competitors’ probes.
The great news: ASHRAE has recently extended the ranges in that chart, giving you a tolerance that allows you to safely save on energy costs—as noted above, up to 4% for every degree raised.
What’s even cooler (no pun intended)—you can put your own temperature and humidity parameters into Power IQ. That’s useful because many server manufacturers have re-engineered their products in recent years to handle harsher environments. Some have even certified their servers to run in 90-to-95-degree environments. You can take those manufacturer’s settings now and incorporate them into your ASHRAE Psychrometric chart. Now you can selectively raise your air temperature and save more on energy.
With the global view of temperatures you get from Power IQ, you can see where you’re over-provisioned or under-provisioned across rows, aisles, and even multiple data centers. You can even see where you’re pumping too much CO2 into the air. Now there’s a feature that’s not only good for your bottom line; it’s the right thing for the environment.
But there’s more: Because Power IQ can actually report on how much CO2 emission has been reduced, that metric yields dollar savings as well. Do a search on “data center energy rebates” and you’ll see that if you can document your CO2 reduction, many energy providers will give you a lower rate.
Being able to say you’ve reduced CO2 emissions by W, kWh by X, power costs by Y, and lowered rates by Z percent will make you a hero in your data center.
Also, Power IQ has joined the great mobile migration. If you want to be not only alerted but empowered to take action if the temperature around a certain server exceeds a certain threshold, there’s a Power IQ app for that. You can get an alert that while you’re away from the data center and proceed to power cycle the affected device, right from your iPhone.
Click here to learn more about Raritan data center power solutions
Dorothy Ochs
April 25, 2013
Raritan has a limited number of complimentary passes available (for end users only) for the DCD Washington show taking place on May 2nd. Contact us to get your free pass.
We will also have live demos in our booth (#TCB) and a raffle drawing for an iPad mini. Hope you can join us.
For more details, visit http://www.datacenterdynamics.com/conferences/2013/washington-dc-2013
April 25, 2013
Key Note Speaker:
EDI, Ltd.‘s Jeremy Gilbertson, CTS, RCDD
Topics Covered:
Jeremy Gilbertson, CTS, RCDD is Vice President of EDI, Ltd.‘s Data Center Practice and is responsible for overall strategic direction, management, and project delivery for the practice. Jeremy’s expertise involves helping enterprise, third-party provider, healthcare, and higher-education clients understand the current state of their data centers and develop phased strategies that address business requirements, risk profile, and budget.
Join us for an afternoon of leading edge Data Center discussions and real world case studies ranging from design through intelligent infrastructure management followed by a tasting of the best brews and appetizers.
When:
Thursday, May 23rd from 12:00pm-5:00pm
Where:
Gordon Biersch Brewery (Buckhead location)
3242 Peachtree Road N
Atlanta GA 30305
Case Studies on Tap:
About EDI, Ltd. EDI, Ltd. is a leading healthcare IT consulting and design firm specializing in medical communication technologies, information systems infrastructure, security, audio-visual systems, and data center.
Attendees will be entered into a drawing for a Kindle Fire!
Space is limited.
Henry Hsu
April 23, 2013
Last week, Raritan shipped our first production run of—what we believe to be—the highest-density rack power strip in the industry to date.
Like all other Raritan rack power strips sold in North America, these units are UL Listed (bear the true UL Listed Mark). They will be placed in cabinets that will obviously get very hot, so like all Raritan power strips with the part number prefix “PX2”, these units have a maximum ambient temperature of 140°F (60°C) in North American markets.
Although the customer application is confidential, generally speaking, this power strip could easily handle up to twelve blade chassis (with common configurations) in a Tier IV environment:
**This is meant as a generalization. Please be sure to consult your Raritan power architect for more detailed provisioning guidance.
Today, the status quo for cabinet densities tends to be approximately 5 to 10 kW. Raritan has been very fortunate to have partnered with some of the industry’s most forward-thinking data center operators and architects—and have thus designed and deployed a significant number of different power strip configurations at higher densities. For electrical reasons, they cluster in the 14kW, 25kW, 28kW, 33kW, and now 55kW ranges.
It’s a great deal of fun, and I enjoy advising clients on the best way to deploy ever-increasing power densities at a minimal cost.
Here are some more photos, if you’d like to take a closer look:
Please note:
I am obligated by law to mention that this power strip happens to be from Raritan’s PX2-4000 Series—which means that in addition to supplying an absurd amount of power, it also provides billing-grade (+/- 1%) kWh energy metering for every inlet, breaker, and individual outlet [C13 and C19]. It is compatible with our wide variety of environmental sensors (temp, humidity, differential air pressure, leak, door open/close); Wi-Fi (802.11a/b/g/n) options; daisy-chaining; USB mass configuration; etc. And it can be queried via either SNMP v1/2c/3 or JSON-RPC.
But enough with the infomercial… fundamentally, I just think it’s awesome to have a single rack PDU that delivers the equivalent amount of power as consumed by five average U.S. homes.
Dorothy Ochs
April 19, 2013
Join us as we discuss how to successfully deploy high power to your racks, and full power chain and network connection management
Stop by our booth (#835) to see our newest Power, DCIM and KVM solutions
Get a registration discount on us—Use code RARITANS13 Register Now - http://www.datacenterworld.com/spring2013/
Deploying High Power at the Rack
Date: Tuesday, April 30 from 8:15 to 9:15 am
Room: Palm D
Speaker: David Wood - Director, Power Business at Raritan
Full Power Chain and Network Connection
Date: Wednesday, May 1 from10:00 to 11:00 am
Room: Banyan CD
Speaker: James Cerwinski - Manager, Project Management at Raritan
We will have live demos at our booth (#835) and will be raffling an iPad. Be sure to stop by!