Home » Raritan Blog
Paula Alves
July 9, 2015
Catch the free replay of the webinar moderated by IDC on July 16, 2015 2PM EST
IDC’s Jennifer Koppy leads an interactive webinar with data center leaders at UF Health Shands Hospital and CareTech Solutions. Learn how to get buy-in from stakeholders, breakdown silos, increase collaboration, and slash 50% on data center OPEX. Discover how to drive change from day one, and set yourself up for more success well into the future.
To watch the replay click on the link below.
Minder Singh
July 6, 2015
In environments that have high amounts of activity, it is very easy for power cords to become loose and fall out. If this happens, it can be dangerous to your equipment, environment and overall business. To prevent this from happening, Raritan has three options: push-button locking outlets, retention clips and Raritan’s SecureLock power cables mated to Raritan SecureLock ready rack PDUs. The push-button locking outlets and retention clips allow you to use your existing power cords, while the SecureLock option requires the purchase of SecureLock cables.
Michael Bord
June 25, 2015
Get to know Raritan's new AV-over-IP (RAV-IP) Distribution System. It provides high-performance video and audio streaming over flexible, low-cost IP networks. Raritan’s simple encoder and decoder based system can be installed in minutes using low-cost Cat5/6 cable, fiber, and Gigabit Ethernet switches. The system is unique in its flexible support for both Cat5 and fiber in a single system.
Yuka Ibara
June 19, 2015
We are proud to announce that Raritan's PX3 intelligent rack PDU series has won the Grand Prize for the Best of Show Award at INTEROP Tokyo 2015 .
What is the Best of Show Award? According to Interop Tokyo's English website, juries of IT experts evaluate the latest products, solutions, and services from a field of over 400 companies at organization that are exhibiting. The winners and finalists are representative of IT trends of the year. According to the judges, "The PDU development concept is filled with LOVE for Power. We are touched by that love, so the PX3 deserves the grand prize. We hope you will keep on showering Power with as much love as you can." See photos from the event after the jump.
Michael Bord
June 12, 2015
It doesn’t look like much at first glance. You notice a row or two of electrical outlets that run the length of a metal box. A small LCD screen (compared to say, your iPhone 6), various ports, and a few buttons. Some funny markings: L3/L1, L2/L3, L1/L2. It’s the sort of machine a real gearhead loves. But, not the kind those of us dependent on ‘technology consumerization’ can appreciate. You want to like it, but you’re not sure what to make of this thing from the outside.
Here’s the funny thing about it though. This box full of blinking lights and whirring noises is the most sophisticated device in the data center power distribution chain. That’s not an exaggeration. Let’s start with a quick recap of the intelligent PDU's capabilities.