Home » Raritan Blog
Michael Bord
November 10, 2015
As 2015 comes to a close, experts predict data center consolidation will become a priority in the forthcoming year. This is partly in anticipation of the strain that the internet of things (IoT) will put on data centers. But it is also reactive. Several companies have already felt the bite of greater power and cooling demands eating into profits. And there’s also the issue of high realty costs. For data centers in prime geographic areas, there’s an immediate need to make better use of existing space.
Sanjay Motwani
October 21, 2015
Imagine a data center in New York or Shanghai or Bangalore for that matter, looking at expansion. With leases and rentals hitting the roof, what is the most economical way for them to expand? A horizontal growth will only incur additional expenses of cabling, cooling and not to mention gigantic real estate. Adding to the operating cost can only put pressure on the bottom-line. Data centers have a continuous need to look at ways to be cost effective in order to get a competitive edge in the crowded market space. With the realty rates reaching the sky, data centers are challenged to maximize benefits from existing space without impacting their expansion plans. If this sounds like a complex problem, the solution is simple – find ways that provide more computing power for less cost per square foot. Now, the question is how do we put this simple solution to work? The answer lies in vertical expansion powered by the right choice of power distribution units.
Greg More
September 16, 2015
As you can imagine, a wide variety of rack power distribution unit (PDU) configurations are available based on parameters such as: number of phases, voltage, total amps, branch circuits, number of outlets, socket type, plug type, rack units consumed, and physical dimensions. Beyond the functions of the basic rack PDU, additional capabilities are available in rack PDU categories we call metered, switched, and intelligent PDUs.
Furthermore, if you cannot find an off-the-shelf rack PDU that matches your specific requirement, some vendors will assemble or even design a custom rack PDU (also called BTO/ETO: built-to-order/engineered-to-order). Here, we'll discuss seven basic steps you should follow to help you to select and deploy the appropriate rack PDUs for your data center.
Michael Bord
August 25, 2015
Jon Inaba
August 20, 2015
Photo: Upcoming Forth Worth Data Center
Want to dramatically reduce your CAPEX spend on your next data center buildout? Consider deploying hardwired rack power distribution units (rack PDUs). Typical savings for a 60A/208V environment are in excess of $1000 per rack.