About Us

Raritan’s Power IQ Energy Management Software Talks to More Enterprise Systems and Manages More Data

Posted on January 13, 2010

—New Release is also Certified VMware-Ready, and Supports 5,000 PDUs and Web Services Integration—

SOMERSET, N.J. (January 13, 2009) – To improve operational and energy efficiency in data centers, Raritan today announced added systems integration capabilities to its Power IQ™ data center energy management software and support for more data center equipment.  Power IQ helps companies track and analyze energy usage down to the individual IT device level and implement energy-saving actions from a central power console.

Power IQ’s new Web Services APIs—Power Control API and Configuration Item API—enable customers to integrate Power IQ with their existing enterprise systems, such as HP Asset Management, as well as build custom tools.  A customer, for example, can write Web service scripts to automate power control to support their unique operational needs.  “Power IQ enables customers to manage their data centers smarter,” said James Cerwinski, Senior Product Manager in Raritan’s Power Business Unit.  “Now with the new Web Services APIs, we provide customers a way to implement their creative ideas to manage their enterprise’s power.”

At North Carolina-based WebAssign, for example, Power IQ is helping the company reduce costs and manage its data center with fewer resources.  “Power IQ allows me to manage and forecast easily my power needs in the data center for optimal efficiency and uptime,” said Matt Pusateri, Systems Administrator at WebAssign, the leading provider of online instructional tools for faculty and students.  “I can also look in one place to obtain energy usage reports and to do firmware upgrades of our Raritan intelligent rack PDUs—rather than having to visit each PDU individually.  Additionally, the centralized aggregation of my power consumption will be invaluable in planning future data centers, and analyzing future power needs.”

Power IQ—which collects and analyzes energy data of IT equipment connected to Raritan and third-party Ethernet-enabled intelligent rack power distribution units (PDUs)—now supports APC and Liebert UPSs.  “Not all IT equipment is connected to rack PDUs,” explains Cerwinski.  “Some equipment, such as routers and disk arrays, is connected to rack UPSs or directly to floor UPSs.  Power IQ now enables a UPS to be a source for power data collection, which helps provide a more complete picture of IT power consumption in a lab or data center.”

The new release of Power IQ also supports deployments of up to 5,000 rack PDUs, making it the most scalable Energy Management Virtual Appliance on the market.  In addition to collecting data from Dominion PX’s environmental sensors for analyzing rack temperature and humidity information, PowerIQ now collects data from Server Technology rack PDU probes and NetBotz.  Power IQ also gathers power information on IT equipment connected to ‘not-so-smart’ PDUs using Raritan’s Dominion PX-3000 inline power meters, which are designed to be used in conjunction with dumb rack PDUs to provide comprehensive strip-level metering on all types of IT equipment.

Power IQ recently achieved VMware certification and is designated “VMware Ready.”  Many customers deploy Power IQ as a virtual appliance because it helps save rack space, energy, and hardware costs.  Power IQ is also offered as a hardware appliance.   

Enterprise-wide data collection at the device level enables Power IQ’s analytics to calculate and chart active power, energy consumption, cost, and carbon footprint for servers and other IT devices.  Power information is presented in user-configurable graphs and reports that can be accessed from anywhere with Power IQ’s Web-based dashboard.  Graphs can easily depict which devices are consuming the most energy, whether power conservation efforts are working, and if there are hot spots or over-cooled areas.  Remedial steps —such as scheduling devices to turn off for periods when not needed or increasing a server room’s ambient temperature gradually —can be made easily using Power IQ’s remote power management capabilities.

Availability

Power IQ 1.5 is available now through Raritan’s channel partners; and is available in English, Japanese, Simplified Chinese, German and French.  To learn more and download a free 5-device version, visit: http://www.raritan.com/products/power-management/power-iq/

Power IQ received key industry recognition recently with a CRN Tech Innovator Runner-Up Award in the Business Software Enterprise category.

About Raritan (Raritan.com)

Raritan is a proven innovator of power management, infrastructure management, KVM, and serial solutions for data centers of all sizes.  In more than 50,000 locations worldwide, Raritan’s award-winning hardware and software solutions—including intelligent PDUs, energy management software, KVM-over-IP, and Serial-over-IP access products—provide IT and facility directors, managers, and administrators with the control they need to increase power management efficiency, improve data center productivity and enhance branch office operations. Based in Somerset, N.J., Raritan has offices worldwide serving 76 countries.  For more information, visit Raritan.com.

Raritan is an active member of the Green Grid, Climate Savers Computing Initiative, and the Leadership in Energy and Environmental Design associations.  The company was recently recognized by the EPA for its contribution to the agency’s data center initiative.
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on April 1, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021