About Us

Raritan Extends Reach of Remote Server Management with New KVM Product

Posted on November 26, 2018

SOMERSET, NJ (November 21, 2018)Raritan® — a brand of Legrand, and a leading provider of intelligent data center management and rack power distribution solutions — today added a new solution, the Cat5 Reach DVI HD KVM Extender, to its portfolio to extend up to 3,300 feet the reach of KVM management to servers, PCs, and other devices. The extended access-and-control capabilities provide more flexibility and boost productivity.

The solution includes a transmitter and receiver pair for use with a Cat5 cable.  By plugging a keyboard, video, and mouse into the Raritan Extender receiver, IT administrators can place the user console anywhere from 330 to 3,300 feet away from the target server or device to be managed.  IT administrators, for example, can use the Extender to access equipment in a nearby control room or an area adjacent to a data center. 

The Extender’s remote access-and-control capabilities also help minimize risk by enabling users to store PCs, servers, and KVM switches in secure, non-harsh environments, as well as eliminate physical trips to equipment rooms.

Like other Raritan offerings, the KVM Extender delivers high quality HD video resolution for a great user experience.  With 1080p HD video-quality resolution, it is almost impossible to differentiate whether you are working in front of a server or in another location away from the server rack. The Extender also provides superior 1920x1200@60Hz and 1080p@60fps (frames per second). video quality.

“Our KVM solutions are designed to help IT teams manage more — servers, devices, locations, technology platforms — manage more efficiently, and do it securely and from anywhere it is convenient,” says Raritan Director Richard Dominach.  “It’s a huge productivity boost for IT administrators.”

Top Raritan Cat5 Reach DVI HD Features:

  • Supports DVI, VGA and audio output
  • Provides dual console support enabling local and/or remote control
  • Extends keyboard, video and mouse signals from 330 to 3300 feet (via IGMP and Jumbo frame’ Ethernet switch daisy-chaining)
  • Supports a wide range of configurations and Raritan KVM switches. Also supports USB devices, such as touch screen, USB Printer, USB barcode reader, USB thumb drives

The Raritan Cat5 Reach DVI HD is available worldwide through Raritan’s extensive distribution channel.

About Raritan’s KVM Portfolio
Raritan’s KVM switches can be found in data centers around the world. Designed for customers requiring secure server access from anywhere, Raritan flagship KVM switch, the Dominion KX III, enables multiple IT administrators — remote and local users — to access multiple servers. They provide BIOS-level access, so that all servers, including blades, are always accessible— even if a server’s operating system is not working. The KX III also enables remote installation of software, file transfers, data backup and diagnostics with its Universal Virtual Media feature, and can control power to servers with optional remote power strips. The Dominion KX III includes security features such as a FIPS 140-2 certified cryptographic module, smart-card/CAC authentication, and IPv6. And with dual power supplies and dual gigabit Ethernet ports, the Dominion KX III is the most reliable and secure digital KVM switch in the industry.

About Raritan
Raritan, a brand of Legrand, is a global leader in intelligent rack PDUs, KVM switches, and other data center infrastructure monitoring and management solutions. Raritan’s innovations improve the reliability, efficiency, and intelligence of data centers and server rooms around the globe — including those of the top Fortune 500 companies, such as Cisco, Dell, Google, HP, IBM, Intel, and Microsoft. To learn more, visit Raritan.com, LinkedIn or Twitter.

About Legrand and Legrand, North and Central America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Sanus, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.

# # #

All product and company names herein may be trademarks of their registered owners.

View by Category
Monthly Archives
More Recent News
Legrand Wins Back-to-Back Awards for Intelligent Rack Power Distribution Innovation
Posted on May 24, 2024
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on April 1, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021