About Us

Raritan Adds New Swappable Sensor and Mini Plug-in Sensor for Monitoring Data Center Environments

Posted on December 3, 2013

—New tiny plug-in MINI sensor requires no cables and new swappable-sensor product measures three spots recommended by ASHRAE—

SOMERSET, N.J. (December 3, 2013) – Raritan, a leading provider of data center infrastructure management (DCIM) and rack power distribution solutions, today added two new sensor models that are easy and quick to deploy for monitoring temperature among racks and keeping IT equipment healthy. Requiring no cabling, Raritan’s new DPX-T1-MINI sensor measures ambient temperatures in the hot aisle side of a rack.  Similar in size to a USB stick, the tiny sensor takes only a few seconds to install because it plugs directly into the sensor port of a Raritan intelligent rack power distribution unit (iPDU).  Plugging a sensor into a Raritan iPDU — the first with a built-in sensor port—eliminates the need for a separate controller or cabling, which helps reduce costs and simplifies deployment.

Raritan’s new four-sensor product, DPX2-T3H1, is also easy to deploy because the multiple sensors are pre-connected to one cable.  Designed to measure temperature and humidity on the cool-air inlet side of a server rack, the new combo sensor makes it easy to follow ASHRAE’s (American Society of Heating, Refrigerating and Air-Conditioning Engineers) cooling guidelines for sensor placement at the top, middle, and bottom of a rack.  To make maintenance easier, the DPX2-T3H1 comes with replaceable sensor heads.  If needed, a sensor can be easily swapped out for a new sensor head—eliminating the need and cost to remove and replace the entire sensor product.

“Raritan is focused on adding intelligent monitoring to data center racks so that they can be managed more efficiently and run optimally.  It all boils down to having the right management and feedback tools to support the care and feeding of IT assets in racks,” said David Wood, Director of Power Management Solutions at Raritan.  “With today’s new offerings, data center managers are able to monitor temperature and humidity and to get accurate information in order to increase temperature safely and eliminate the cost of over cooling data centers.  We continue to focus on making solutions useful to data center professionals and that are easy to deploy and maintain.”

A Web-based GUI enables data center managers to monitor remotely the sensors and report and plot sensor values in real-time or over a period of time.  Environmental information also can be shared with DCIM solutions, such as Raritan’s Power IQ® energy management software.  Sensors connect to the network by plugging into Raritan’s iPDUs, which, in turn, connect to the network via Ethernet or Wi-Fi.

Raritan’s sensor portfolio includes temperature, humidity, airflow, air pressure, water and contact closure, as well as asset tracking sensors.  To learn more about Raritan’s environmental and infrastructure monitoring solutions, visit http://www.raritan.com/environment-management/.

About Raritan

Raritan is a proven innovator of energy and infrastructure management solutions for data centers of all sizes.  In more than 50,000 locations worldwide, Raritan’s award-winning hardware and software solutions—including intelligent rack PDUs and sensors; DCIM and energy management software; and access and control products—provide IT and facility directors, managers, and administrators with the control they need to increase power management efficiency, improve data center productivity and enhance operations.  Based in Somerset, N.J., Raritan has offices worldwide serving customers in 76 countries.  Visit us at Raritan.com or follow us on the Raritan blog.

Raritan is an active member of the Green Grid, Climate Savers Computing Initiative, and the Leadership in Energy and Environmental Design associations.  The EPA has recognized Raritan for its contribution to the agency’s data center initiative.  A number of top industry analyst firms also have recognized the company:  Raritan was named a “Cool DCIM Vendor” by Gartner; a “Major DCIM player worldwide” by IDC; a “Strong Value DCIM Vendor” by EMA; and, “Key DCIM player” by TechNavio.

View by Category
Monthly Archives
More Recent News
Legrand Wins Back-to-Back Awards for Intelligent Rack Power Distribution Innovation
Posted on May 24, 2024
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on April 1, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021