About Us

Microsoft’s Enterprise Engineering Center Selects Raritan’s IT Infrastructure and Power Management S

Posted on May 11, 2009

SOMERSET, NJ (May 11, 2009) - Raritan today announced that Microsoft’s Enterprise Engineering Center (EEC) has chosen a suite of Raritan IT infrastructure management solutions for monitoring servers and their energy consumption down to the outlet level.

Located on the main Microsoft campus in Redmond, Washington, the state-of-the-art data center contains more than $125 million in hardware and networking equipment, and houses multiple labs for Microsoft’s enterprise customers to collaborate with product teams to test and validate Microsoft software solutions in replicas of customer production environments.

The EEC will use Raritan’s remote access and control solutions - including Raritan’s Dominion® KX II KVM-over-IP switches and CommandCenter® Secure Gateway - to configure and transform each lab into a scaled representation of a customer’s infrastructure.  From any Web browser, administrators, as well as customers, will be able to control and configure servers and other IT equipment.  The KX II provides secure BIOS-level access with Absolute Mouse Synchronization to servers and supports remote installation of software and diagnostics.

In addition, Raritan’s new power management solutions will help customers analyze power consumption and cooling requirements for different server configurations.  Servers in the labs will be plugged into Raritan’s Dominion PX intelligent rack Power Distribution Units (PDU), which measure power consumption at the outlet level.  “With the Dominion PX we’ll be monitoring daily the amount of amperage and watts drawn by each piece of equipment in our server racks,” said Microsoft EEC Business Development Manager Steve Cole.  “We also will be able to look at cooling and humidity statistics at the racks using the Dominion PX environmental sensors.”

Raritan’s intelligent PX PDUs also will help the EEC find valuable free rack space by using real-time power draw information of equipment instead of relying upon nameplate data.

“The remote management capabilities of the PX, as well as the Dominion KX, are key enablers of zero-touch automated machine deployment,” added Cole.  “The PX, for example, gives us the ability to remotely power on servers, which is done in sequence to prevent a massive power draw at boot-up.  It also helps us in reducing the EEC’s energy costs by enabling us to remotely turn off servers that are not in use.”

“We are pleased to support Microsoft’s Enterprise Engineering Center and its customers,” said Gary Marks, Raritan Vice President of Sales and Marketing.  “Raritan’s solutions will help customers in testing and validating their simulated environments, as well as give them an opportunity to test the energy efficiencies of their configurations.”

About Raritan (Raritan.com)

Raritan provides secure IT infrastructure management solutions that increase data center efficiency and productivity by delivering integrated in-band and out-of-band energy management, server access and control.  Raritan’s power management software, intelligent PDU, environmental sensors, KVM, serial console and centralized management products are in use in more than 50,000 locations worldwide. Raritan’s OEM division provides embedded hardware and firmware for server and client management, including intelligent energy management, KVM over IP, IPMI and other industry standards-based management applications.  Based in Somerset, N.J., Raritan has offices worldwide serving 76 countries.  For more information, please visit Raritan.com
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on April 1, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021