Posted on September 27, 2011
SOMERSET, N.J. (September 27, 2011)—Raritan today announced the Smart Rack Controller (EMX) that provides, in one place, key information on data center operations collected from many types of sensors—including temperature, humidity, airflow, air pressure, smoke, water, and contact closure—from cameras, and from Raritan’s just-introduced intelligent, electronic asset tracking solution.
At a glance, operators can see if their data center is working at an optimal temperature, monitor humidity and airflow in racks, locate a server’s exact location, and see live views of the data center. They can detect when a cabinet door is opened, see who has entered the data center and be alerted if there is a problem—such as smoke or a security breach.
Posted on September 9, 2011
—Raritan DCIM solutions, including first-of-its-kind intelligent asset management tags and sensors, shown at AFCOM Data Center World—
SOMERSET, N.J. (September 9, 2011)—Raritan executives are scheduled to speak at Data Center World next week in Orlando, Fla. The Raritan sessions focus on best practices and tools for delivering optimal operations and managing data centers resources more efficiently—including IT and facilities equipment, rack space and energy.
Monday, September 12, 9:45–10:45am
Improve Data Center Capacity Utilization (Session P06)
Khaled Nassoura, General Manager of the Green Data Center Initiative, Raritan
Posted on August 29, 2011
—Accurate, automated, real-time inventory; helps data centers better understand exactly what they have and where it’s located—
SOMERSET, N.J. (August 29, 2011)—Raritan today announced the general availability of the first intelligent Asset Management Tag and Sensor solution for improving data center asset management by providing accurate, real-time information on all IT assets and their locations.
With a large number of IT devices and a great variety of equipment, data center moves, adds, and changes are challenging. Accurate records on where servers are located in racks and the power chain associated with servers are not always available. In fact, in larger data centers up to 25 percent of IT assets can go missing because of difficulty tracking IT assets. This translates into underutilized rack space and capacity, contributes to ghost servers, as well as wasted time locating equipment.
Posted on July 12, 2011
—Smart Racks, True kWh Energy Metering and Secure Outlet-level Switching with New PX-2000 Series—
SOMERSET, N.J. (July 12, 2011) – With the introduction of the PX-2000 family, Raritan today expanded the industry’s largest portfolio of intelligent rack power distribution units (iPDUs) that make server racks a lot smarter. Its built-in intelligence provides real-time monitoring of data center energy and loads, as well as environmental conditions when using optional plug-in sensors.
The PX-2000 outlet-switched rack iPDU measures energy usage at the PDU level and provides outlet-level switching to shut down and turn on IT equipment remotely. PX-2000 models are available for 120V, 208V, three-phase 208V, three-phase 400V, 16A and less, 20A and 30A.
Posted on July 6, 2011
—New release of Dominion® KX II delivers a number of industry firsts; First Smartphone/Tablet KVM-over-IP solution, in-browser KVM client, and end-to-end digital audio over IP—
SOMERSET, N.J. (July 6, 2011)—Raritan today introduced the first KVM-over-IP switch that enables the use of Smartphones and tablets to manage remote servers. Using Apple iPhones® and iPads®, IT administrators on the go can obtain secure BIOS-level access to servers being managed by Raritan’s Dominion® KX II release 2.4 and CommandCenter®-Secure Gateway release 5.2.