Home » Raritan Blog
April 30, 2024
Whenever data center operators or other companies that employ mission-critical services purchase a product to go in their data centers, there’s a tick-in-the-box exercise to confirm that the product conforms to various international standards and certifications. For example, our Raritan PX4 Rack PDUs have been tested and conform to FCC Part 15 Class A, UL and cULs, IEC 62368, CE, UKCA as standard certifications. (Additional certifications are available).
September 20, 2023
We’re excited to announce that the new Raritan Secure Switch 4.0 is now available! It’s equipped with two, four, and eight ports, with CAC authentication now standard on all models. Some new models now include dual monitor support as well.
February 14, 2023
As businesses increasingly rely on technology, data centers have become essential to today’s operations. These centers house and manage the servers and other technology that keep companies running smoothly. However, with the increasing amount of sensitive data stored in data centers, it is crucial to ensure proper security measures are in place.
Jessica Ciesla
October 18, 2021
Raritan offers a large portfolio of rack Power Distribution Units (PDUs) with more than 700 models to choose from. Despite all those options, some companies have unique data center requirements and need custom PDU solutions. That’s where Raritan’s Advanced Engineering team comes in.
Jessica Ciesla
October 1, 2021
The world is driven by software is not a shocking claim, but the ubiquity of its presence is worth a reminder. A recent hunt for a new refrigerator served as a notification, in case I had forgotten, about the pervasive nature of the IoT and the ability to connect to just about anything, even an appliance, from anywhere you have an internet connection. The same holds true for our large modern data center networks, obviously, from building automation and controls packages right down to the software operating intelligent rack PDUs.