The Raritan Blog

Who Should Care About ISO 27001?

April 30, 2024

Whenever data center operators or other companies that employ mission-critical services purchase a product to go in their data centers, there’s a tick-in-the-box exercise to confirm that the product conforms to various international standards and certifications. For example, our Raritan PX4 Rack PDUs have been tested and conform to FCC Part 15 Class A, UL and cULs, IEC 62368, CE, UKCA as standard certifications. (Additional certifications are available). 


The Rapid Growth of AI and the Use of Raritan PDUs to Meet Higher Power Demands

Marc Cram
October 11, 2023

You have to hand it to the folks at Gartner. When they began using and promoting the term' hype cycle', it was an insightful description of the collective hysteria that seems to take place around every innovation from the technology community. Today, the world is abuzz with the terms "ChatGPT," "Artificial Intelligence," and "AI."


Data Center Report Fewer Outages, But Downtime Still Costly

September 20, 2023

Data center operators say the number and severity of outages have decreased in the past few years. However, when significant outages do occur, the costs remain significant.


Survey: Energy Usage and Staffing Shortages Challenge Data Centers

September 20, 2023

Data center operators say their most pressing management concerns are finding ways to reduce energy consumption and dealing with a persistent IT staff shortage, a new survey by the Uptime Institute shows.


Raritan Secure Switch: Secure NIAP 4.0 Compliant Desktop KVM

September 20, 2023

We’re excited to announce that the new Raritan Secure Switch 4.0  is now available! It’s equipped with two, four, and eight ports, with CAC authentication now standard on all models. Some new models now include dual monitor support as well.


Page 1 of 93 pages  1 2 3 >  Last ›