部落格

PDU Mass Deployment and Lifecycle Management

Posted on November 29, 2016 by Gento

You recently acquired brand new PDUs or you are in the process of evaluating power distribution solutions. You are probably asking yourself: “How can I easily and seamlessly deploy my PDUs and leverage their capabilities in my existing DCIM software or BMS?”

Well look no further.  I’m here to give you a quick overview of Raritan’s open API and scripting capabilities, as well as our mass configuration options.  

Our PX2 and PX3 intelligent rack PDUs leverage JSON RPC to easily configure your PDU to your exact requirements.  JSON RPC is a simple protocol that binds major coding languages like Python, Perl, and JavaScript to your PDU functionalities.

JSON RPC allows you to automate PDU features like outlet-level switching, or access power data, environment info, alarms, and thresholds. In turn, you can integrate rack-level data into the GUI of commercial and homegrown DCIM and BMS systems.  Pretty neat, huh?

But the best part is you don’t have to start from scratch. Our PX2 and PX3 support pages offer a downloadable Software Development Kit (SDK) with pre-integrated bindings.  From there, you’re free to customize those scripts to meet any unique needs.

On the mass configuration side, we offer two great options. The first is a traditional network based deployment option; the second is by using USB Flash drives.

Raritan PDUs use common protocols to enable you to remotely control and access your PDU through the Network. With DHCP/PXE and SSH protocols, your PDU is automatically recognized on a network as soon as its Ethernet port is connected.  This allows you to safely boot and push the desired configuration through a TFTP Server.

As an added note, Secure Shell (SSH) protocol is automatically embedded. This allows you to securely and remotely save and restore your initial configuration (individually or in bulk across your data center], and manage backups, firmware upgrades, and system restores over the network.

A few years ago, Henry Hsu discussed how to rapidly configure intelligent rack PDUs, so I won’t get into the specifics of the feature on this blog post.  But, I would like to share an incredible case study from a client who recently used the feature to deploy his PDUs.

For the first stage, they opted to configure their PDUs via the traditional method of connecting to each device and configuring via CLI. For the second stage they opted to use Raritan's USB configuration method. Note the difference: 

Phase One – Four techs, sixteen hours, and 200 PDUs via serial management port/CLI worked out to $1,600 USD.

Phase Two – Two techs, two hours, and 200 PDUs via USB mass deployment method (includes bar coding, creating the confiq file, cross referencing customers IP address, subnet and alarms) worked out to only $200 USD.  A cost reduction of 87.5%! 

To learn more about these features, please watch the video above.


You can also learn more about the PX series of rack PDUs here, or ask us a question.

Other Blog Posts

誰該關心 ISO 27001?
Posted on July 1, 2024
從資料中心失效對企業帶來的骨牌效應──探討感測器的重要性
Posted on November 5, 2023
更高規格的電源要求加速AI市場成長與Raritan PDU的採用
Posted on October 11, 2023
資料中心服務中斷次數減少,但停機的代價仍舊可觀
Posted on September 20, 2023
意見調查:資料中心面臨能源使用與人力短缺困境
Posted on September 20, 2023

View all Blog Posts

訂閱

近期活動

New Zealand Cloud & Datacenter Convention 2022
3 November 2022, 9am – 4pm  •  Grand Millennium Hotel, Auckland, New Zealand
Data Centre World Singapore
12th – 13th Oct 2022
Korea Cloud & Datacenter Convention 2022
6th Oct 2022
Philippines Cloud & Datacenter Convention 2022
4th Aug 2022
JANOG50 Meeting Hokkaido
3th – 15th July 2022

View all Events

Raritan最新新聞

—ISO27001 認證為 Legrand 羅格朗品牌(包括 Raritan®、Server Technology® 和 Starline® 品牌)經過徹底測試的數據、電源和控制設備的安全性提供了保證。
Posted on July 1, 2024
Legrand 使用兩大創新智慧型機架 PDU 重新活化資料中心產業
Posted on May 1, 2023
Exclusive interview丨How does Huizhou upgrade its manufacturing industry?
Posted on December 2, 2021
Raritan 發表 MasterConsole® 數位雙電腦切換器
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020

View all news