Posted on July 12, 2011
—Smart Racks, True kWh Energy Metering and Secure Outlet-level Switching with New PX-2000 Series—
SOMERSET, N.J. (July 12, 2011) – With the introduction of the PX-2000 family, Raritan today expanded the industry’s largest portfolio of intelligent rack power distribution units (iPDUs) that make server racks a lot smarter. Its built-in intelligence provides real-time monitoring of data center energy and loads, as well as environmental conditions when using optional plug-in sensors.
The PX-2000 outlet-switched rack iPDU measures energy usage at the PDU level and provides outlet-level switching to shut down and turn on IT equipment remotely. PX-2000 models are available for 120V, 208V, three-phase 208V, three-phase 400V, 16A and less, 20A and 30A.
Posted on July 6, 2011
—New release of Dominion® KX II delivers a number of industry firsts; First SmartPhone/Tablet KVM-over-IP solution, in-browser KVM client, and end-to-end digital audio over IP—
SOMERSET, N.J. (July 6, 2011)—Raritan today introduced the first KVM-over-IP switch that enables the use of SmartPhones and tablets to manage remote servers. Using Apple iPhones® and iPads®, IT administrators on the go can obtain secure BIOS-level access to servers being managed by Raritan’s Dominion® KX II release 2.4 and CommandCenter®-Secure Gateway release 5.2.
Posted on June 13, 2011
—Company also recognized with eBay for ‘Environmental Project of the Year’ award—
SOMERSET, N.J. (June 13, 2011) – Raritan today announced that its data center management solutions have received multiple awards recently from industry organizations around the globe. Raritan’s solutions that help data centers better manage and utilize resources were selected for the innovative ways they solve data center energy issues—such as reducing energy waste, finding capacity, and more-efficient ways to add servers and make changes.
Posted on May 24, 2011
—dcTrack Version 2.5 software’s change, capacity and asset management tools help maximize data center efficiency and find stranded capacity—
SOMERSET, N.J. (May 24, 2011) – Raritan today introduced new data center infrastructure management (DCIM) tools to help managers easily find available space, power and network connectivity within their data centers in order to add or change IT equipment. The new web-based tools in dcTrack DCIM software Release 2.5, which is available worldwide starting today, help data center managers obtain the most from their existing capacity.
Posted on May 10, 2011
—New real-time power gauge finds stranded capacity—
SANTA CLARA, CA (May 10, 2011) – Raritan today unveiled a new configurable dashboard with new tools and gauges for Power IQ® energy management software, so that data center managers can easily see information most important to them—whether it’s energy usage information of a specific server rack, temperature readings from the cold aisle, or a forecast on how much energy is required to support operations in data centers across the world.
The Power IQ energy dashboard displays complex information in easy-to-view reports, charts, thermal graphs, and maps. The new capacity forecast chart, for example, provides “days of supply” information and helps determine the available power at any level—data center, floor, room, row or rack. Power IQ also provides real-time information on energy usage, energy costs, carbon footprint, and thermal factors.