The Raritan Blog

Keep it Safe: Overload Protection at the Rack

Posted on September 22, 2021 by Gento

This article from Raritan provides an overview of overload protection standards for rackmount PDUs.   

Lost in most discussions about rackmount PDUs and intelligent PDUs is a simple premise: their job is to keep you and your equipment safe. Newly certified ITE PDUs of any type and with more than 20 amps are required to use overcurrent protection that meets branch circuit protection requirements in accordance with the National Electrical Code, ANSI/NFPA 70. In effect, this means these products are required to have branch circuit breakers listed under UL 489, “Standard for Molded-Case Circuit Breakers, Molded-Case Switches and Circuit Breaker Enclosures,” or fuses listed for branch circuit protection, such as those listed under UL 248-5, “Low-Voltage Fuses – Part 5: Class G Fuses.” 

Using the Right Circuit Breaker Means Avoiding Short-Circuit Disasters 

In addition to UL Standard 489, Underwriters Laboratories also publishes UL Standard 1077, which is the “Standard for Supplementary Protectors for Use in Electrical Equipment.” Devices certified to this standard are considered “Supplementary Protectors” and are called “Recognized” components, not “Listed” devices (as UL 489 breakers are). UL Listed Circuit Breakers meet more stringent requirements for branch circuit protection than Supplementary Protectors with UL Recognition. UL 489 requires the breaker to be functional after being subjected to a short-circuit test. UL 1077 and the IEC standard EN 60934 allow for breakers to clear a short-circuit condition but become safely destroyed in the process. 

Circuit breakers are used in a variety of ways: 

  • They are mounted in panel boards (also referred to as building PDUs) and rackmount PDUs to protect branch-circuit wiring. 
  • They are also built into equipment to protect components and systems. Interrupting a short circuit—current flow limited only by the resistance of wiring—is a severe test of a circuit breaker. 
  • If the interrupting capacity of the breaker is not adequate, the device could literally explode. 

While that last bullet sounds a little dramatic, it is a friendly reminder that the amount of energy being harnessed in the electrical systems of most data centers, even at the rack or individual circuit level, is significant. Keep in mind UL 489 breakers can interrupt short circuits of 5,000 amps or more and UL 1077 breakers can interrupt fault currents of 1,000 amps. 

Overload Protection and Rack Mount PDUs 

If you would like more information on the topic of data center overload protection, check out our White Paper “Data Center Power Overload Protection: Circuit Breakers and Branch Circuit Protection for Data Centers”. 

Contact us here at Raritan to learn more about how our rackmount PDUs can support your power safety needs. 

Other Blog Posts

Chief Data Center Concerns Going Into 2025
Posted on February 27, 2025
Improving Rack Power Quality with Innovative PDUs
Posted on February 27, 2025
Solving the Problem of the Data Center Digital Twin
Posted on July 11, 2024
2024 Will be a Big Year for Greater Analytics Automation in the Data Center. Here’s How
Posted on July 2, 2024
Who Should Care About ISO 27001?
Posted on July 1, 2024

View all Blog Posts

Subscribe

Upcoming Events

New Zealand Cloud & Datacenter Convention 2022
3 November 2022, 9am – 4pm  •  Grand Millennium Hotel, Auckland, New Zealand
Data Centre World Singapore
12th – 13th Oct 2022
Korea Cloud & Datacenter Convention 2022
6th Oct 2022
Philippines Cloud & Datacenter Convention 2022
4th Aug 2022
JANOG50 Meeting Hokkaido
3th – 15th July 2022

View all Events

Latest News

Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications
Posted on July 1, 2024
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs
Posted on May 1, 2023
Exclusive interview丨How does Huizhou upgrade its manufacturing industry?
Posted on December 2, 2021
Raritan Reveals The MasterConsole® Digital Dual KVM Switch
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020

View all news