Home » The Raritan Blog
Posted on May 6, 2019 by Gento
Did you know that data centers consume approximately 1.8 percent of the total United States' electricity consumption? This unprecedented energy usage is expected to increase year over year as the amount of data consumed on an annual basis rises at unparalleled rates. The inherent challenge of rising energy and data consumption levels lies in environmental monitoring. In fact, when IT equipment isn't operated in the right environment (including within the designated temperature safe zone) it can lead to disastrous results.
Posted on April 25, 2019 by Gento
Load balancing can be a tricky and confusing procedure to understand. As its name suggests, load balancing focuses on evenly distributing current draw throughout the entire rack. The goal is to achieve perfect balance so that more total current can be supplied to each branch circuit.
Posted on April 18, 2019 by Gento
With each passing year data center power infrastructures become more complex. In fact, data is expected to reach an unprecedented 163 zettabytes by 2025, which means that data center operators must figure out how to a) support the additional data, b) reduce costs, c) increase efficiencies, and d) remain energy efficient. Fortunately, data center operators can address the latter challenges with the help of the advanced power metering and data management technologies found in Intelligent PDUs.
Posted on April 4, 2019 by Gento
The Dominion KX IV-101 represents the latest in a long series of innovations from the Raritan team. In fact, the Dominion KX IV-101 is our fourth generation Dominion KVM-over-IP switch. It delivers an unparalleled level of power, supports Java-free access from anywhere, and offers BIOS-level remote access to PCs, workstations, and servers. With 4K video resolution at up to 30 frames per second in 4🔢2 color, the Dominion KX IV-101 redefines the remote management that many businesses need to thrive.
Enjoy The Most Popular Dominion Features
The beauty of the recently released Dominion KX IV-101 is that it allows businesses to enjoy un-blocked, high performance access to equipment via the Dominion User Station, PCs, or laptops. This impressive KVM-over-IP switch also allows users to enjoy the most popular Dominion features, including:
Posted on March 25, 2019 by Gento
Data centers throughout the globe are constantly finding new ways to innovate. More often than not, these innovative approaches stem from a growing need to reduce unexpected downtime, increase efficiencies, streamline operations, and optimize the entire data center for future growth. While you most often hear about enhancements to DCIM solutions or the benefits of intelligent rack PDUs, one topic that isn't covered as often are outlet types including C21 / C22.