Posted on July 15, 2014
—Patent-Pending Hybrid Design Delivers Fast and Reliable Power Load Transfer Performance—
SAN FRANCISCO (May 19, 2014)—Raritan, a leading provider of data center infrastructure management (DCIM) and rack power distribution solutions, today introduced the Intelligent Rack Transfer Switch (PX3TS) to help keep data center equipment operating through power failures. When the new switch senses power loss, it provides fast and seamless power load transfers from one power source to another without interrupting operations.
The PX3TS switch—which was announced today at Cisco Live, Cisco’s annual IT and communications conference—is targeted at cloud computing infrastructures and data center racks filled with one-power-supply devices.
Raritan’s PX3TS switch uses an innovative hybrid design to provide fast power loss detection and load transfers that exceed that of other offerings in the market, including standard automatic transfer switches (ATS), and at a lower price point and greater energy efficiency than static transfer switches.
By sampling the current 4,800 times per second with built-in sensors, the Raritan switch transfers the load within four to eight milliseconds. To deliver fast performance and reliability, Raritan’s patent-pending hybrid design uses the best of both electromechanical relay and silicon-controlled rectifier (SCR) technologies.
“Every millisecond counts when there is a power failure,” says Greg More, Senior Product Marketing Manager at Raritan. “Our new hybrid rack transfer switch is one of the fastest in the industry—twice as fast as standard automatic transfer switches, which take from 10 to 16 milliseconds to transfer loads.”
The new Raritan Transfer Switch also provides remote monitoring and PDU unit-level metering to support capacity planning decisions and to utilize power resources efficiently. Real-time power information gathered by the switch can be easily shared with Raritan’s DCIM software solution for monitoring and managing the health of the rack and the data center.
Availability
Available worldwide, the Raritan Transfer Switch PX3TS comes with a number of options and a range of voltage and plug types. The PX3TS switch comes with an intelligent network-ready controller with display, and with two USB-A and one USB-B ports to support Wi-Fi networking, webcams and cascading to share IP drops. The switch’s sensor ports support optional Raritan plug-and-play sensors for monitoring environmental conditions in the racks.
About Raritan
Raritan is a proven innovator of energy and infrastructure management solutions for data centers of all sizes. In more than 50,000 locations worldwide, Raritan’s award-winning hardware and software solutions – including intelligent rack PDUs and environment sensors; DCIM software; and KVM switch products – provide IT and facility directors, managers and administrators with the control they need to increase power management efficiency, improve data center productivity and enhance operations. Based in Somerset, N.J., Raritan has offices worldwide serving customers in 76 countries. Visit us at Raritan.com, RaritanDCIM.com, or follow us on the Raritan blog.
Raritan is an active member of the Green Grid, Climate Savers Computing Initiative, and the Leadership in Energy and Environmental Design associations. The EPA has recognized Raritan for its contribution to the agency’s data center initiative. A number of top industry analyst firms also have recognized the company: Raritan was named a “Cool DCIM Vendor” by Gartner; a “Major DCIM player worldwide” by IDC; a “Strong Value DCIM Vendor” by EMA; and, “Key DCIM player” by TechNavio.
# # #
All marks are the property of their respective owners.